Other Parts Discussed in Thread: SPRC090
Hello,
I've attached a project showing a problem I'm seeing. I imported a project from CCS3.3 to CCS 5.2.1 using the legacy import option. When I'm building my program, it gives me an error saying the linker can't find a *cfg.cmd file. The file exists but it isn't being looked for in the right place.
To match my project location, extract the zip file to C:\Docs. The project is called MatMult. The current configuration is 'SPM6420_Debug'. The include and lib paths are only correct for this configuration. Also, the C6000 CSL (SPRC090) is needed and is assumed to be installed at the default location: 'C:\Program Files\C6xCSL'.
Please let me know if you need any more information.
Sincerely,
Josh