This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem allocating large vectors in C6x compiler

I am having problem allocating large memory in C6x compiler. Below is the main code to illustrate the problem
#define PANELSIZE (128)
#define NUMBERPANEL (64)
#define MATRIXSIZE (PANELSIZE*NUMBERPANEL)
#pragma DATA_SECTION(matrix, ".data")
#pragma DATA_ALIGN(matrix, 128)
double matrix[MATRIXSIZE*MATRIXSIZE];
#pragma DATA_SECTION(vector, ".data")
#pragma DATA_ALIGN(vector, 128)
double vector[MATRIXSIZE];
void main(void) {
int i;
for(i=0;i<MATRIXSIZE*MATRIXSIZE;i++) matrix[i] = (double) i;
for(i=0;i<MATRIXSIZE;i++) vector[i] = (double) i;
}
 
The linker file is below
-heap 0x1000
-stack 0x1000
MEMORY
{
L2SRAM (RWX) : org = 0x00800000, len = 0x00080000
MSMCSRAM (RWX) : org = 0x0c000000, len = 0x00400000
DDR3 (RWX) : org = 0x80000000, len = 0x40000000
}
 
SECTIONS
{
.stack > L2SRAM
.sysmem: > L2SRAM
.data: > DDR3
GROUP: > L2SRAM
{
.bss:
.neardata:
.rodata:
} 
.cinit: > L2SRAM
.const: > L2SRAM
.data: > L2SRAM
.fardata: > L2SRAM
.switch: > L2SRAM
.far: > L2SRAM
.cio: > L2SRAM
}
 
When I compile the above (compiler version 7.4.1) , I see the memory allocation for matrix and vector as follows in the map file

80000000 matrix

80000000 vector

Thus matrix and vector overlap; zero bytes are allocated for matirx

If I change the NUMBERPANEL to 63, The map file shows the following allocation of matrix and vector showing correctly allocated bytes for matrix

80000000 matrix

9f020000 vector

It appears the compiler is wrapping around 2^29 for large allocation size.

Murtaza