This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using Boost libraries with C6670

Hello,

    I am trying to run someone else's C++ code on a C6670 EVM.  This code presupposes Boost library support.  There is a Texas Instruments wiki entry on this topic but there isn't enough information on the wiki to actually be able to use the Boost library.   I downloaded version 1.34.1 of the Boost code as indicated in the wiki.  I also used the ti.hpp and user.hpp files the wiki provided.   The problem is I am trying to run this using SYS/BIOS.  The wiki entry seems to indicate the BOOST_NO_PLATFORM_CONFIG #define can be set and the code will work.  The compiler generates an error if BOOST_NO_PLATFORM_CONFIG is defined. It wants you to choose a platform and SYS/BIOS is not a recognized platform.  Any ideas or help would be appreciated.

 Thanks