Hi,
I am developing the h.263 decoder with the CCS v5.2.1. When I imported and built the TI's example project "c66x_m4h3dec_02_03_00_01_ELF", I got the following errors:
This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.
warning: relocation to symbol "ECPY_directStartEdma" overflowed; the 22-bit relocated address 0x10f49e is too large to encode in the 21-bit signed PC-Relative field (type = 'R_C6000_PCR_S21' (4), file = "...\Lib\m4h3dec_ti_le66", offset = 0x000209b8, section = ".text: M4H3DEC_TI_cSect1")
warning: relocation to symbol "ECPY_directConfigure" overflowed; the 22-bit relocated address 0x10f49e is too large to encode in the 21-bit signed PC-Relative field (type = 'R_C6000_PCR_S21' (4), file = "...\Lib\m4h3dec_ti_le66", offset = 0x0002f4ec, section = ".text: M4H3DEC_TI_cSect1")
DIAG/user_msg_api.c: 211: internal fatal error #99926: (ofile_error_handler(): TestAppDecoder.out: illegal operation: writing 0x1ffff384 bytes to offset 0x0 in section ".text" exceeds its formatted size (0xa6360))
Internal ERROR: C:\ti\ccsv5\tools\compiler\c6000_7.3.4\bin\lnk6x.exe aborted.
This is a serious problem. Please contact Customer Support with this message and a copy of the input file and help us to continue to make the tools more robust.
However, the example project runs successfully with CCS v4.
Please help me.
Thanks and Best regards!