Hi,
we have a problem using the RTS function getenv() over JTAG since CCS 5.3.0. It seems that CCS writes beyond the CIO buffer as soon as the DSP reaches the breakpoint within writemsg():
In Version 5.2.1.00018 it works as expected with the same binary.
These are my conditions:
- Hardware: C6415
- Host: Windows 7 64 Bit
- CG Tools: 7.3.8, rts6400.lib
- Emulator: SD XDS510 USB Plus
Thanks,
Ralf