I tried to update the Code Composer Studio v5.3.0.00090 by using the "Check for Updates" menu but this did not work.
My OS: Windows 7 Professional 64 bit.
CCS 5.3.0 is the only CCS version installed on this PC (I uninstalled the previously installed CCS 5.2.0 version before installing CCS 5.3.0).
First error was, that the available updates were shown (see the figure below) with the conflict "Cannot complete the install because of a conflicting dependency" because of some conflicting components (here the "Eclipse Help System v 1.4.1" and "Eclipse Platform 3.8.1"). In my opinion this is an error since the automatic update should not select conflicting components.
The problem of conflicting dependency occured also for some other components, e.g. for "Remote System Explorer End-User Runtime" and "Target Management Terminal":
Then, I just deselected all components but one ("Autotools support for CDT") and started the update. After a few seconds, I got the following "No repository found containing" error message (see also the figure below):
After that I tried some other components to update. Only "Spectrum Digital Emulator" update was working. The other updates (I did not test all components but some of them) were always failing with the "No repository found containing...." error.
Are some Eclipse repositories down or not working properly?