Hi,
Debugging under CCS... I run via F8 (Resume I think, I just use the keyboard shortcuts all the time)... sometimes I want to "re-run" or restart, basically from the reset vector... but the only reliable way I've found is to exit the tool and re-start (!!!)
I've tried various commands under "Run" -- Restart, "Go Main", and both versions of "Reset" (Core & System).
What is the proper command sequence to accomplish this?
Also, if anyone can point me to where in the documentation this is explained, that would be great.