Hi,
I'm connecting to a DM6437 board successively using the spectrumdigital XDS510 USB emulator but I cant read the memory I'm getting "----" instead of the memory content, the memory map looks good and the EVM test connection also pass,
I'm using CCSv5.2.0.00069 under windows XP, I have CCS3.3 installed on the same machine and it is working fine, what could be the issue?
Thanks,
HR