I have looked at examples ,but they do not have a full linker command file to show how it is done,
can anyone show how the CRC is generated for this command file
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
.text
ZONE0 : origin = 0x002000, length = 0x002000 /* XINTF zone 0 */
ZONE1 : origin = 0x004000, length = 0x002000 /* XINTF zone 1 */
RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */
ZONE2 : origin = 0x080000, length = 0x080000 /* XINTF zone 2 */
ZONE6 : origin = 0x100000, length = 0x080000 /* XINTF zone 6 */
OTP : origin = 0x3D7800, length = 0x000800 /* on-chip OTP */
/* modified to place CRC */
APPCRC : origin = 0x3E8000, length = 0x000020 /* CRC of user app on-chip FLASH */
FLASHE : origin = 0x3E8020, length = 0x003FE0 /* on-chip FLASH */
/* FLASHE : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHD : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
/* ZONE7 : origin = 0x3FC000, length = 0x003FC0 /* XINTF zone 7 available if MP/MCn=1 */
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM available if MP/MCn=0 */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
SIZE(_code_size), /* added*/
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > RAML1 PAGE = 1
.esysmem : > RAMH0 PAGE = 1
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHD PAGE = 0
.switch : > FLASHD PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHC PAGE = 0 /* Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
/* This did not work*/
UNION
{
.cinit:
.pinit:
.text:
} crc_table(table1, algorithm=CRC32_PRIME)
}