Hi,
I have a application ( u-boot). It has been built with debug symbols. ( has application.out and application file ( symbols file).
When i do a load symbols and point to application file, i do not see any symbols. Is it a ccs issue?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a application ( u-boot). It has been built with debug symbols. ( has application.out and application file ( symbols file).
When i do a load symbols and point to application file, i do not see any symbols. Is it a ccs issue?
thanks
Hi Faraday,
can you please provide more information. Normally if you do a full symbolic build a .out file is generated that will include symbols. After loading the code a first time you should be able to do a Load Symbols only as you describe. I say after loading the code a first time as the symbols and code on the device should line up for things to make sense.
What steps are you taking? Have you done a full symbolic debug? What are you experiencing that you write you "do not see any symbols"?
Best Regards,
Lisa