Hello,
C6accel currently in, I have added the original function.
Additional modules I have been describing in cpp (c + + code), INTERNAL ERROR occurs when you write a std :: vector <int>. compilation is completed without error occurs when you write new int in [].
How do I do I do?
I want to add a function that is being written in c + + code.
TMS320C6000 C/C++ CODE GENERATION TOOLS v7.3.4
CCS v5.2
----- console log ------------
======== .executables [packages/ti/c6accel_unitservers/TI816X/] ========
lnke674 bin/ti_platforms_evmTI816X_DSP/ti816x.xe674 ...
INTERNAL ERROR: /home/pal/ti-ezsdk_dm816x-evm_5_04_00_11/dsp-devkit/cgt6x_7_3_1/bin/lnk6x failed to allocate memory
This is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.
gmake[1]: *** [bin/ti_platforms_evmTI816X_DSP/ti816x.xe674] エラー 2
make[1]: ディレクトリ `/home/pal/projects/c6accel_custom/soc' から出ます
gmake: *** [packages/ti/c6accel_unitservers/TI816X/,.executables] エラー 2
make[1]: *** [server] エラー 2
make: *** [c6accel] エラー 2