Hello,
I was running an update on my CCS 5.2.1 from whatever was found in Help->Check for updates, it downloaded everything and installed, but loading the workspace and converting the projects ended with a "Waiting for user operation" forever box, which I closed and restarted CCS. Now the projects are loaded, but run another update and some Eclipse platform updates were applied. After another restart, another check for update and now I receive a "The operation could not be completed. See the details" with the following error message:
Cannot complete the install because of a conflicting dependency.
Software being installed: Eclipse Help System 1.4.1.v20120726-051048-8R7xFOUFLWUl7MoSKV_RBXl27 (org.eclipse.help.feature.group 1.4.1.v20120726-051048-8R7xFOUFLWUl7MoSKV_RBXl27)
Software currently installed: Eclipse Platform 3.8.1.M20120914-1540 (org.eclipse.platform.ide 3.8.1.M20120914-1540)
Only one of the following can be installed at once:
Help System Base 3.6.100.v201209141800 (org.eclipse.help.base 3.6.100.v201209141800)
Help System Base 3.6.1.v201109091335 (org.eclipse.help.base 3.6.1.v201109091335)
Help System Base 3.6.2.v201202080800 (org.eclipse.help.base 3.6.2.v201202080800)
Help System Base 3.6.0.v201106131736 (org.eclipse.help.base 3.6.0.v201106131736)
Help System Base 3.6.100.v201206081400 (org.eclipse.help.base 3.6.100.v201206081400)
Help System Base 3.6.100.v201206081200 (org.eclipse.help.base 3.6.100.v201206081200)
Help System Base 3.6.100.v201209141540 (org.eclipse.help.base 3.6.100.v201209141540)
Cannot satisfy dependency:
From: Eclipse Help System 1.4.1.v20120726-050831-8R7xFOUFLWUl7MoSKV_OFXl27 (org.eclipse.help.feature.group 1.4.1.v20120726-050831-8R7xFOUFLWUl7MoSKV_OFXl27)
To: org.eclipse.help.base [3.6.100.v201209141540]
Cannot satisfy dependency:
From: Eclipse Help System 1.4.1.v20120726-051048-8R7xFOUFLWUl7MoSKV_RBXl27 (org.eclipse.help.feature.group 1.4.1.v20120726-051048-8R7xFOUFLWUl7MoSKV_RBXl27)
To: org.eclipse.help.base [3.6.100.v201209141800]
Cannot satisfy dependency:
From: Eclipse Platform 3.8.1.v20120815-074604-9gF7jI7wG5qDyZMWGg8NPvDbfWFWlIJU-kYaOQ (org.eclipse.platform.feature.group 3.8.1.v20120815-074604-9gF7jI7wG5qDyZMWGg8NPvDbfWFWlIJU-kYaOQ)
To: org.eclipse.help.feature.group [1.4.1.v20120726-050831-8R7xFOUFLWUl7MoSKV_OFXl27]
Cannot satisfy dependency:
From: Eclipse Platform 3.8.1.M20120914-1540 (org.eclipse.platform.ide 3.8.1.M20120914-1540)
To: org.eclipse.platform.feature.group [3.8.1.v20120815-074604-9gF7jI7wG5qDyZMWGg8NPvDbfWFWlIJU-kYaOQ]
Also see the image of available updates. Is this supposed to happen? I don't have any other Eclipse instance or any PC development tools on my system.
My environment is Windows 7,
biospsp_03_00_01_00
bios_6_33_05_46
bios_6_34_02_18
C6748_StarterWare_trunk
ccsv5
dsplib_c674x_3_1_1_1
edma3_lld_02_11_06_01
ipc_1_24_03_32
ipc_1_25_00_04
mathlib_c674x_3_0_1_1
uia_1_01_00_04
uia_1_01_01_14
xdais_7_21_01_07
xdctools_3_23_03_53
xdctools_3_24_05_48
Best regards,
David.