Hello,
I am trying to build a StarterWare application using CCSv5. The CCS version I am using is Version: 5.1.1.00031. The build completes with errors.
The build log is given below.
**** Build of configuration Debug for project dmtimerCounter ****
E:\Program Files\Texas Instruments\ccsv5\CCS5.1.1.00031\ccsv5\utils\bin\gmake -k -j 2 -s all
'Building file: F:/StarterWare Releases/AM335x_StarterWare_02_00_00_07_01_Aug_12/examples/evmAM335x/dmtimer/dmtimerCounter.c'
'Invoking: TMS470 Compiler'
'Finished building: F:/StarterWare Releases/AM335x_StarterWare_02_00_00_07_01_Aug_12/examples/evmAM335x/dmtimer/dmtimerCounter.c'
' '
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/dmtimer/dmtimerCounter.out'
'Invoking: TMS470 Linker'
<Linking>
'Finished building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/dmtimer/dmtimerCounter.out'
' 'process_begin: CreateProcess(E:\Program, E:/Program Files/Texas Instruments/ccsv5/CCS5.1.1.00031/ccsv5/utils/bin/gmake --no-print-directory post-build, ...) failed.
make (e=193): Error 193
gmake:***[../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/dmtimer/dmtimerCounter.out] Error 193
gmake: Target `all' not remade because of errors.
**** Build Finished ****
As it is observed, the compiling and linking happens successfully. However there is a problem with the function call CreateProcess which happens to be a CCS function.
The first parameter to this function is a path which seems to be cut short because there is a space after 'Program'. Could this be the issue? However previously I had installed CCS in locations which had spaces in the path names. This project has a post-build step which converts the generated '.out' file to a '.bin' file.
I request any one of you to suggest me as to what is going wrong.
Thanks for your effort in advance.
Thanks and Regards.
Gurudutt.