This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS with CCS5

Hi,

At present i am working on 5.3.0.00067  and trying to download a program of TM570LS 3137 and facing below problem in loading file.

I have added some Functions to TMS570LS31 CCS Example provided in CCS 5.3 and tried to download the new program, but failed.

Same files i was success fully build on CCS 3.2 and download through now flash.

Please help me in resolving this.

Thanks for support  in advance.

Regards,

PriyaPost

  • Priya,

    Are you loading via a script?

    Can you try opening the Debug View.  View -> Debug.  Generally closing the debug view can cause problems as it controls the debug context.

    I would suggest opening the Debug View.  Making sure the CortexR4 is selected in the Debug View.  Then trying to load the program via the toolbar.

    I can try to track down a TMS570LS31 but that would be next week.

    Regards,

    John