Other Parts Discussed in Thread: LM3S6965, SYSBIOS
Hello Support:
I have a Stellaris LM3S6965 Eval Board.
I created a new project and essentially copied & pasted the "Timers" project into it. Simple stuff.
I receive this error message.
<Linking>
"./configPkg/linker.cmd", line 203: error: placement fails for object ".resetVecs", size 0x3c (page 0). Available ranges:
FLASH size: 0x40000 unused: 0x3ff10 max hole: 0x3ff10
error: errors encountered during linking; "STMain.out" not built
The following is the memory map. I tried to get everything updated with regards to patches; but, there is a failure on one of the updates.
******************************************************************************
TMS470 Linker PC v4.9.0
******************************************************************************
>> Linked Thu Dec 27 16:03:30 2012
OUTPUT FILE NAME: <STMain.out>
ENTRY POINT SYMBOL: "_c_int00" address: 00004b31
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
FLASH 00000000 00040000 00007b9f 00038461 R X
SRAM 20000000 00010000 00004550 0000bab0 RW X
SEGMENT ALLOCATION MAP
run origin load origin length init length attrs members
---------- ----------- ---------- ----------- ----- -------
00000000 00000000 0000003c 0000003c r--
00000000 00000000 0000003c 0000003c r-- .resetVecs
00000000 00000000 00007ba8 00007ba8 r-x
00000000 00000000 000000f0 000000f0 r-- .intvecs
000000f0 000000f0 00005cce 00005cce r-x .text
00005dc0 00005dc0 00001ba1 00001ba1 r-- .const
00007968 00007968 00000240 00000240 r-- .cinit
20000000 20000000 00003f44 00000140 rw-
20000000 20000000 00000140 00000140 rw- .vecs
20000140 20000140 00002000 00000000 rw- .stack
20002140 20002140 00001e04 00000000 rw- .bss
20003f44 20003f44 0000060c 0000060c rw-
20003f44 20003f44 0000060c 0000060c rw- .data
I've tried to follow the other folks that had similar issues and could not translater their "fixes" into something that was menaingful for me.
What else do you need in order to help diagnose the issue?
Thanks
Rick