Hello,
I am trying to implement chorus effect in C using intrinsic function and I need a little help with it. I pasted a link for a file containing the code and if it is possible tell me if it is ok cause I cant find any example match this one.Its maide by LFO with cosine with 8192 samples due to modulo adressing.
Input: f s= 48kHz, 16 bit
chorus: delay = 30ms, modulation +- 10ms, gain = 0.707
THX much. I need it fast so if it is possible many thanks to you.