Looks like my CCS 3.3 instalaltion has problems displaying the disassembly. It does not seem to be able to parse packed 16-bit instructions, all instructions are 32-bit. Target is c674x. CGT installed 6.1.2[0-2] 7.3.[2-8] 7.4.1
Is this known and if so is there a workaround?
Note: the (somehow) same setup works on another win7 64bit setup.
May there be issues with the 7.x compiler versions installed? They are not used with CCS, as not selected in component manager.
Thank you!