Other Parts Discussed in Thread: MSP-EXP430FR5739, MSP430WARE
How can I correct the section allocation map? How does it get populated? I've detected some differences in the section allocation maps between two files (attached).
1680.MSP-EXP430FR5739_UserExperience.zip
The two files are from two different projects. Both have the same C code. Project 123 works. Project MSP-EXP430FR5739_UserExperience does not. I could not find any project settings that can account for this difference in Code Composer Studio. I discovered that the interrupt labels are missing and the stack is missing from project MSP-EXP430FR5739_UserExperience.
If you want to recreate the problem here is my setup:
Code Example imported through Code Composer Studio resource explorer from MSP430Ware (single click):
C:\TI\ccsv5\ccs_base\msp430\MSP430ware_1_30_00_15\examples\boards\MSP-EXP430FR5739\MSP-EXP430FR5739 User Experience
Code Composer Studio Version: 5.3.0.00090 (used for both projects; the one that works, and the one that does not)
Hardware: MSP-EXP430FR5739
In order to create project 123, I just started a new Code Composer Studio project and copied the contents from the example above.