Hi,
I want to install the Linux CCS v5.0.3 which comes with the EVMC6678 board, to Ubuntu 12, X32. There is a help file named README_FIRST.txt on the Windows/Linux OS. It says that after untar setup_CCS_5.0.3.xxxxx.tar and extract all files, run setup_CCS_5.0.3.xxxxx.bin (Linux). The problem here is that there is no file named: setup_CCS_5.0.3.xxxxx.bin (Linux)
After the extraction, I can see there is text file: README_FIRST.txt and two folders: extras and install_images. I check the two folders as well for setup_CCS_5.0.3.xxxxx.bin. There is no such setup_CCS_5.0.3.xxxxx.bin in those folders.
Could you help me?
Thanks