This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5.3 installed on Linux OPENSUSE 12.1 64bit as root or user mode?

Hi,

I try installing CCS v5.3 on Linux OPENSUSE 12.1, 64 bit as the link procedures:

http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/151119/585202.aspx#585202

When the dialogue box asks for install path, it says I have no permission after I select to /opt/ti path. I try to select /usr/blackhawk/ti, it seems it can continue (but I abort it before I get confirmed this has no trouble later).

As a superuser, I try to install CCS v5.3 as root mode.It has no response first:

linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux # ./ccs_setup_5.3.0.00090.bin &
[1] 6678

Then, when I press enter key, it shows:


linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux #

[1]+  Stopped                 ./ccs_setup_5.3.0.00090.bin

That is, the installer does not response (no install window shows up) in superuser mode. In user mode, it cannot be installed to /opt/ti path.

This problem is normal or not? Please give your advice.

Thanks

  • Could you run this without the "&" to make sure we're seeing all the console output?

  • Hi,

    In user mode, if there is no @ at the end, it refuses to install. It seems that it only installs in the background.

    .................

    blackhawk@linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux> sudo ./ccs_setup_5.3.0.00090.bin              
    Please set DISPLAY. Code Composer Studio v5 cannot be installed in console mode.    
    ...................

  • Hi,

    I also check the file modes. It seems both user and root can execute it.

    BTW, what is the meaning of the first letter 'd' in file attributes.

    Thanks,

    ...........

    blackhawk@linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux> l
    total 1912
    drwxr-xr-x 8 root root    4096 Jan 11 06:56 ./
    drwxr-xr-x 3 root root    4096 Jan 11 06:56 ../
    drwxr-xr-x 3 root root    4096 Dec 13 17:13 .artifactlock/
    -rwxr-xr-x 1 root root     717 Dec 13 17:13 artifacts.jar*
    drwxr-xr-x 2 root root    4096 Jan 11 06:56 baserepo/
    drwxr-xr-x 2 root root    4096 Jan 11 06:56 binary/
    -rwxr-xr-x 1 root root 1904687 Dec 13 17:13 ccs_setup_5.3.0.00090.bin*
    -rwxr-xr-x 1 root root    2141 Dec 13 17:13 content.jar*
    drwxr-xr-x 4 root root    4096 Jan 11 06:56 featurerepo/
    drwxr-xr-x 2 root root    4096 Jan 11 06:56 features/
    drwxr-xr-x 2 root root    4096 Jan 11 06:56 plugins/
    -rwxr-xr-x 1 root root    1975 May 25  2012 README_FIRST.txt*
    -rwxr-xr-x 1 root root      16 Dec 13 17:12 timestamp.txt*

  • What is your DISPLAY environment variable set to?

    "d" is a folder.

    Please, see this post.

  • At user mode, I get DISPLAY variable is:

    blackhawk@linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux> echo $DISPLAY
    :0
    blackhawk@linux-iu5j:/tmp/ccsv5_install/CCS5.3.0.00090_linux>

  • I'm having a similar problem, but with openSUSE 12.2. Attempting to SUDO run the installer gives:

    Please set DISPLAY. Code Composer Studio v5 cannot be installed in console mode.

    My $DISPLAY is the same as blackhawk's, above

    :0