hi
I am using ccs and i installed control suite along with it.I bought a Dc Dc developer kit and peripheral explorer kit and jtag along with it.I would like to know whether it is possible to add example codes from control suite to load in to the kits and provide some codes which would verify whether the kits are working properly.I have loaded a code in to peripheral kit but i don't know how to verify whether it is loaded in to it or not.It was an example code for the control card that i was using on the kit.And i am using usb 2000 to load and debug the code.
Regards
Arun