Hi,
Previously, I downloaded 5.0.3.00028 CCS from : http://processors.wiki.ti.com/index.php/Download_CCS and installed it on Ubuntu 12.1.
I find that the pdk_C6678_1_1_2_5 example project cannot build. I suspect that CCS version is different from the bundled DVD ROM. I extract setup_CCS_5.0.3.00028.tar.gz to hard disk.
The README_FIRST.txt file says:
(2) On Linux,
(a) Untar setup_CCS_5.0.3.xxxxx.tar and extract all files
(b) Run setup_CCS_5.0.3.xxxxx.bin (Linux) and follow the installation instructions
but I cannot find one such setup_CCS_5.0.3.xxxxx.bin file. Under CCS_5.0.3/install_images folder, there are these files:
They look like the component programs. How do I begin with for installation?
Thanks,