Other Parts Discussed in Thread: SYSBIOS
Hello.
I created a project for dm355 processor using BIOS and Codec Engine. But the building fails. The following are the sources and project settings.
// - - - - - - - - - - - - - hello.c - - - - - - - - - - - - - - - - - - - - -
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sdo/fc/dskt2/dskt2.h>
#include <ti/sdo/ce/utils/syscbuf/SysCBuf.h>
#include <xdc/std.h>
#include <ti/sdo/ce/Engine.h>
#include <ti/sdo/ce/CERuntime.h>
Void main()
{
System_printf("hello world\n");
CERuntime_init();
BIOS_exit(0);
}
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var Memory = xdc.useModule('xdc.runtime.Memory');
var SysCBuf = xdc.useModule('ti.sdo.ce.utils.syscbuf.SysCBuf');
var Engine = xdc.useModule('ti.sdo.ce.Engine');
var Settings = xdc.useModule('ti.sdo.ce.osal.bios.Settings');
var Server = xdc.useModule('ti.sdo.ce.Server');
var UNIVERSALConfig = xdc.useModule('ti.sdo.ce.universal.UNIVERSALConfig');
xdc.useModule('ti.sysbios.xdcruntime.Settings');
Program.argSize = 0x0;
BIOS.heapSize = 0x2000;
Program.stack = 0x1000;
SysMin.bufSize = 0x400;
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 32;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
var tempMemParams = new HeapMem.Params();
var extHeapName = "DDR2"; // just a default, override if needed
tempMemParams.size = 0x00400000; // 4 MB
tempMemParams.sectionName = ".DDR2_HEAP";
Program.global.DDR2_HEAP = HeapMem.create(tempMemParams);
Program.sectMap[".DDR2_HEAP"] = extHeapName;
var osalGlobal = xdc.useModule('ti.sdo.ce.osal.Global');
osalGlobal.runtimeEnv = osalGlobal.DSPBIOS;
var CERuntime = xdc.useModule('ti.sdo.ce.CERuntime');
xdc.useModule('xdc.runtime.knl.Thread');
var DSKT2 = xdc.useModule('ti.sdo.fc.dskt2.DSKT2');
DSKT2.DARAM0 = "DDR2_HEAP";
DSKT2.DARAM1 = "DDR2_HEAP";
DSKT2.DARAM2 = "DDR2_HEAP";
DSKT2.SARAM0 = "DDR2_HEAP";
DSKT2.SARAM1 = "DDR2_HEAP";
DSKT2.SARAM2 = "DDR2_HEAP";
DSKT2.ESDATA = "DDR2_HEAP";
DSKT2.IPROG = "DDR2_HEAP";
DSKT2.EPROG = "DDR2_HEAP";
DSKT2.DSKT2_HEAP = "DDR2_HEAP";
Memory.defaultHeapSize = 4096;
// - - - - - - - - - - - - - - - - Build console- - - - - - - - - - - - - - - - - - - - - - - - - - - -
"H:\\CCS 5.3\\ccsv5\\utils\\bin\\gmake" -k all
'Building target: CE_t.out'
'Invoking: ARM Linker'
"H:/CCS 5.3/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv5e --code_state=32 --abi=eabi -me -g --define=dm355 --define=dm350 --diag_warning=225 --display_error_number -z --stack_size=0x800 -m"CE_t.map" --heap_size=0x800 -i"H:/CCS 5.3/ccsv5/tools/compiler/arm_5.0.1/lib" -i"H:/CCS 5.3/ccsv5/tools/compiler/arm_5.0.1/include" --reread_libs --warn_sections --display_error_number --rom_model -o "CE_t.out" -l"./configPkg/linker.cmd" "./hello.obj" -l"libc.a"
<Linking>
warning #10229-D: output section ".data.1" refers to load symbol
"DSKT2_cacheWBInv" and hence cannot be compressed; compression "rle" is
ignored
undefined first referenced
symbol in file
--------- ----------------
Algorithm_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
>> Compilation failure
CESettings_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Comm_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
DSKT2_cacheWBInv G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Engine_alwaysCollectDspTrace G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Engine_ceDebugDspTraceMask G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Engine_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
FCSettings_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Global_getenv G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Global_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Loader_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Processor_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
Server_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
XdmUtils_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
_VISA_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
ti_sdo_ce_osal_Memory_init G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
ti_sdo_ce_utils_syscbuf_SysCBuf_Module_startup__F G:\PVS\prg\CE_t\Debug\configPkg\package\cfg\hello_pe9.oe9
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "CE_t.out" not built
gmake: *** [CE_t.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
I also tried to create a project based on the Codec Engine example, but the result was the same.
Tell me please, is there a possibility of working with Codec Engine for dm355 in CCS. If so, what am I doing wrong?