This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS Version: 4.2.0.10018 keeps freezing / not responding

Hi,

I'm using CCS  Version: 4.2.0.10018 and every few clicks (on whatever) the program locks up and then says "not responding" this lasts for about 30 seconds each time.

In the past it never did this, it's only started doing it recently, but does so all the time.

I've got Eclipse SDK v4.2 (for Android) installed on the same computer, could that have anything to do with it?

I don't think it's a memory issue as when I'm running CCS, the only other program running is Google Chrome

My computer has an Intel Core2Duo CPU @ 2 GHz and 3 Gb of RAM. I'm running Windows 7 Pro SP1.

Any ideas?

Thanks