Other Parts Discussed in Thread: CONTROLSUITE
hi
i am using Code Composer Studio
Version: 5.3.0.00083
Problem does not occur when we try to build from control suite but it does not generate .out file when tries to do from new project.
I am posting the error:
**** Build of configuration Debug for project test1 ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building target: test1.out'
'Invoking: C2000 Linker'
"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/bin/cl2000" -v28 -ml -mt --float_support=fpu32 -g --diag_warning=225 --display_error_number -z --stack_size=0x300 -m"test1.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/include" -i"C:/Users/arun/workspace_v5_3/test1" -i"/DSP2833x_common/lib" -i"/v15c/lib" -i"/V100/lib" --reread_libs --display_error_number --rom_model -o "test1.out" "./main.obj" "./DSP2833x_usDelay.obj" "./DSP2833x_SysCtrl.obj" "./DSP2833x_PieVect.obj" "./DSP2833x_PieCtrl.obj" "./DSP2833x_DefaultIsr.obj" "./DSP2833x_CpuTimers.obj" "./DSP2833x_CodeStartBranch.obj" "./DSP2833x_ADC_cal.obj" -l"rts2800_fpu32.lib" -l"IQmath_fpu32.lib" -l"rts2800_fpu32_fast_supplement.lib" "../28335_RAM_lnk.cmd" "../DSP2833x_Headers_nonBIOS.cmd"
<Linking>
error #10008-D: cannot find file "IQmath_fpu32.lib"
error #10008-D: cannot find file "rts2800_fpu32_fast_supplement.lib"
>> Compilation failure
undefined first referenced
symbol in file
--------- ----------------
_CpuTimer0Regs ./main.obj
_CpuTimer1Regs ./DSP2833x_CpuTimers.obj
_CpuTimer2Regs ./DSP2833x_CpuTimers.obj
_CsmPwl ./DSP2833x_SysCtrl.obj
_CsmRegs ./DSP2833x_SysCtrl.obj
_EPwm1Regs ./main.obj
_FlashRegs ./DSP2833x_SysCtrl.obj
_GpioCtrlRegs ./main.obj
_GpioDataRegs ./main.obj
_PieCtrlRegs ./main.obj
_PieVectTable ./main.obj
_SysCtrlRegs ./main.obj
_XintfRegs ./DSP2833x_SysCtrl.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "test1.out" not built
gmake: *** [test1.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****