I have the AMX 335 demo board and have installed Code Composer from the sd card, when I try to install the ADT from the included archive it fails with the following message:
An error occurred while installing the items
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --> [R]com.ti.ccstudio.base 5.0.0.316, action=com.ti.ccstudio.p2.actions.RunCommanddAction).
Command failed.
I've copied all the dependencies from the cd into my installation directory as per the instructions in the setup guide pdf.
Running Ubuntu 11.10, and compiling with g++ (Ubuntu/Linaro 4.6.1-9ubuntu3) 4.6.1.
The same error message is thrown when installing from the archive included on the sd card with the board and when installing the adt from google's servers.