Hi everyone
There is an option in ccs5's menu which is located in run ->clock->enable. I have a problem using it.
First,click run->clock->setup and set the clock cycle to cpu execute cycle when using a emulator connected to my board.
Then step over,the code is simply nop 1.
I think the clock suppose to add 1 bucause nop 1 take a cpu execute cycle.But the result is not as what i think. It add more than 1 (like 6)when executing nop 1.
1 How to explain this.Does nop 1 take only one cpu execute cycle?
2 How can i get the number of cpu execute cycle that a function takes,or how can i get the executing time of a function?