This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

warning "#10247-D" from CCS

Other Parts Discussed in Thread: MSP430F5529

Hi,

Our customer is having trouble in debugging MSP430F5529 with CCSv5.

There are two Warning messages(below) after compiling the project and
the CCS gives below error when debugging the custom project.
MSP430: File Loader: Data verification failed at address 0x00000000
Please verify target memory and memory map.

Warning messages from CCSv5:
warning #10247-D: creating output section ".data" without a SECTIONS
warning #10247-D: creating output section ".int65530" without a SECTIONS

The problem is solved by placing the above output section sections to FLASH section
in the linker command file.
But we don't know if it is ok to place these into the FLASH section?
and also we don't understand what is ".int65530" and where does it come from
according to my understading there is no such data declared in the program.

I am going to attach the map file of this project.6082.MSP430F5529.txt

Best Regards.
Paddu

  • paddu1 said:

    Warning messages from CCSv5:
    warning #10247-D: creating output section ".data" without a SECTIONS
    warning #10247-D: creating output section ".int65530" without a SECTIONS

    What does their linker command file look like? The default one that gets added when creating new projects in CCS (lnk_msp430f5529.cmd) does allocate the .data section so I would not expect the warning for that section if using that default linker command file. This section is allocated to RAM in that default linker command file.

    Is ".int65530" not a user created section? It would help to look at their linker command file and link map file. Could you please attach both?

  • Thank you.

    Attached is the Linker Command File and the Map file.

    2425.MSP430F5529.txt

    /******************************************************************************/
    /* lnk_msp430f5529.cmd - LINKER COMMAND FILE FOR LINKING MSP430F5529 PROGRAMS     */
    /*                                                                            */
    /*   Usage:  lnk430 <obj files...>    -o <out file> -m <map file> lnk.cmd     */
    /*           cl430  <src files...> -z -o <out file> -m <map file> lnk.cmd     */
    /*                                                                            */
    /*----------------------------------------------------------------------------*/
    /* These linker options are for command line linking only.  For IDE linking,  */
    /* you should set your linker options in Project Properties                   */
    /* -c                                               LINK USING C CONVENTIONS  */
    /* -stack  0x0100                                   SOFTWARE STACK SIZE       */
    /* -heap   0x0100                                   HEAP AREA SIZE            */
    /*                                                                            */
    /*----------------------------------------------------------------------------*/
    
    
    /****************************************************************************/
    /* SPECIFY THE SYSTEM MEMORY MAP                                            */
    /****************************************************************************/
    
    MEMORY
    {
        SFR                     : origin = 0x0000, length = 0x0010
        PERIPHERALS_8BIT        : origin = 0x0010, length = 0x00F0
        PERIPHERALS_16BIT       : origin = 0x0100, length = 0x0100
        RAM                     : origin = 0x2400, length = 0x1800
        INFOA                   : origin = 0x1980, length = 0x0080
        INFOB                   : origin = 0x1900, length = 0x0080
        INFOC                   : origin = 0x1880, length = 0x0080
        INFOD                   : origin = 0x1800, length = 0x0080
        FLASH                   : origin = 0x4400, length = 0xBB80
        FLASH2                  : origin = 0x10000,length = 0x14400
        INT00                   : origin = 0xFF80, length = 0x0002
        INT01                   : origin = 0xFF82, length = 0x0002
        INT02                   : origin = 0xFF84, length = 0x0002
        INT03                   : origin = 0xFF86, length = 0x0002
        INT04                   : origin = 0xFF88, length = 0x0002
        INT05                   : origin = 0xFF8A, length = 0x0002
        INT06                   : origin = 0xFF8C, length = 0x0002
        INT07                   : origin = 0xFF8E, length = 0x0002
        INT08                   : origin = 0xFF90, length = 0x0002
        INT09                   : origin = 0xFF92, length = 0x0002
        INT10                   : origin = 0xFF94, length = 0x0002
        INT11                   : origin = 0xFF96, length = 0x0002
        INT12                   : origin = 0xFF98, length = 0x0002
        INT13                   : origin = 0xFF9A, length = 0x0002
        INT14                   : origin = 0xFF9C, length = 0x0002
        INT15                   : origin = 0xFF9E, length = 0x0002
        INT16                   : origin = 0xFFA0, length = 0x0002
        INT17                   : origin = 0xFFA2, length = 0x0002
        INT18                   : origin = 0xFFA4, length = 0x0002
        INT19                   : origin = 0xFFA6, length = 0x0002
        INT20                   : origin = 0xFFA8, length = 0x0002
        INT21                   : origin = 0xFFAA, length = 0x0002
        INT22                   : origin = 0xFFAC, length = 0x0002
        INT23                   : origin = 0xFFAE, length = 0x0002
        INT24                   : origin = 0xFFB0, length = 0x0002
        INT25                   : origin = 0xFFB2, length = 0x0002
        INT26                   : origin = 0xFFB4, length = 0x0002
        INT27                   : origin = 0xFFB6, length = 0x0002
        INT28                   : origin = 0xFFB8, length = 0x0002
        INT29                   : origin = 0xFFBA, length = 0x0002
        INT30                   : origin = 0xFFBC, length = 0x0002
        INT31                   : origin = 0xFFBE, length = 0x0002
        INT32                   : origin = 0xFFC0, length = 0x0002
        INT33                   : origin = 0xFFC2, length = 0x0002
        INT34                   : origin = 0xFFC4, length = 0x0002
        INT35                   : origin = 0xFFC6, length = 0x0002
        INT36                   : origin = 0xFFC8, length = 0x0002
        INT37                   : origin = 0xFFCA, length = 0x0002
        INT38                   : origin = 0xFFCC, length = 0x0002
        INT39                   : origin = 0xFFCE, length = 0x0002
        INT40                   : origin = 0xFFD0, length = 0x0002
        INT41                   : origin = 0xFFD2, length = 0x0002
        INT42                   : origin = 0xFFD4, length = 0x0002
        INT43                   : origin = 0xFFD6, length = 0x0002
        INT44                   : origin = 0xFFD8, length = 0x0002
        INT45                   : origin = 0xFFDA, length = 0x0002
        INT46                   : origin = 0xFFDC, length = 0x0002
        INT47                   : origin = 0xFFDE, length = 0x0002
        INT48                   : origin = 0xFFE0, length = 0x0002
        INT49                   : origin = 0xFFE2, length = 0x0002
        INT50                   : origin = 0xFFE4, length = 0x0002
        INT51                   : origin = 0xFFE6, length = 0x0002
        INT52                   : origin = 0xFFE8, length = 0x0002
        INT53                   : origin = 0xFFEA, length = 0x0002
        INT54                   : origin = 0xFFEC, length = 0x0002
        INT55                   : origin = 0xFFEE, length = 0x0002
        INT56                   : origin = 0xFFF0, length = 0x0002
        INT57                   : origin = 0xFFF2, length = 0x0002
        INT58                   : origin = 0xFFF4, length = 0x0002
        INT59                   : origin = 0xFFF6, length = 0x0002
        INT60                   : origin = 0xFFF8, length = 0x0002
        INT61                   : origin = 0xFFFA, length = 0x0002
        INT62                   : origin = 0xFFFC, length = 0x0002
        RESET                   : origin = 0xFFFE, length = 0x0002
    }
    
    /****************************************************************************/
    /* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY                              */
    /****************************************************************************/
    
    SECTIONS
    {
        .bss       : {} > RAM                /* GLOBAL & STATIC VARS              */
        .sysmem    : {} > RAM                /* DYNAMIC MEMORY ALLOCATION AREA    */
        .stack     : {} > RAM (HIGH)         /* SOFTWARE SYSTEM STACK             */
    
        .text      : {}>> FLASH | FLASH2     /* CODE                              */
        .text:_isr : {} > FLASH              /* ISR CODE SPACE                    */
        .cinit     : {} > FLASH              /* INITIALIZATION TABLES             */
    //#ifdef (__LARGE_DATA_MODEL__)
        .const     : {} > FLASH | FLASH2     /* CONSTANT DATA                     */
    //#else
    //    .const     : {} > FLASH              /* CONSTANT DATA                     */
    //#endif
        .cio       : {} > RAM                /* C I/O BUFFER                      */
    
        .pinit     : {} > FLASH              /* C++ CONSTRUCTOR TABLES            */
    
        .infoA     : {} > INFOA              /* MSP430 INFO FLASH MEMORY SEGMENTS */
        .infoB     : {} > INFOB
        .infoC     : {} > INFOC
        .infoD     : {} > INFOD
    
        .int00   : {} > INT00                /* MSP430 INTERRUPT VECTORS          */
        .int01   : {} > INT01
        .int02   : {} > INT02
        .int03   : {} > INT03
        .int04   : {} > INT04
        .int05   : {} > INT05
        .int06   : {} > INT06
        .int07   : {} > INT07
        .int08   : {} > INT08
        .int09   : {} > INT09
        .int10   : {} > INT10
        .int11   : {} > INT11
        .int12   : {} > INT12
        .int13   : {} > INT13
        .int14   : {} > INT14
        .int15   : {} > INT15
        .int16   : {} > INT16
        .int17   : {} > INT17
        .int18   : {} > INT18
        .int19   : {} > INT19
        .int20   : {} > INT20
        .int21   : {} > INT21
        .int22   : {} > INT22
        .int23   : {} > INT23
        .int24   : {} > INT24
        .int25   : {} > INT25
        .int26   : {} > INT26
        .int27   : {} > INT27
        .int28   : {} > INT28
        .int29   : {} > INT29
        .int30   : {} > INT30
        .int31   : {} > INT31
        .int32   : {} > INT32
        .int33   : {} > INT33
        .int34   : {} > INT34
        .int35   : {} > INT35
        .int36   : {} > INT36
        .int37   : {} > INT37
        .int38   : {} > INT38
        .int39   : {} > INT39
        .int40   : {} > INT40
        .int41   : {} > INT41
        .int42   : {} > INT42
        .int43   : {} > INT43
        .int44   : {} > INT44
        .int45   : {} > INT45
        .int46   : {} > INT46
        .int47   : {} > INT47
        .int48   : {} > INT48
        .int49   : {} > INT49
        .int50   : {} > INT50
        .int51   : {} > INT51
        .int52   : {} > INT52
        .int53   : {} > INT53
        .int54   : {} > INT54
        .int55   : {} > INT55
        .int56   : {} > INT56
        .int57   : {} > INT57
        .int58   : {} > INT58
        .int59   : {} > INT59
        .int60   : {} > INT60
        .int61   : {} > INT61
        .int62   : {} > INT62
        .reset   : {} > RESET              /* MSP430 RESET VECTOR               */ 
    }
    
    /****************************************************************************/
    /* INCLUDE PERIPHERALS MEMORY MAP                                           */
    /****************************************************************************/
    
    -l msp430f5529.cmd
    
    

    Regards.

    Paddu

  • It looks like they are using an older version of the linker command file(are they using CCS 5.1?) where the .data section allocation is missing. The newer versions of the linker command file included in CCS 5.3 have this section allocated. I have attached the file from CCS 5.3 for your reference. They can simply add the line under SECTIONS that allocates .data.

    As for the .int65530 I am not sure why that is created. We may need to look at their source file int.c for that.

    http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/343/2133.lnk_5F00_msp430f5529.cmd