This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resolved - CCSV5 Re-installation missing install_drivers.sh



Problem:  XSD100 V2 driver not properly installed

1. Un-installing CCSV5.3 (Ubuntu 11.10) via these steps:

$ cd /opt/ti/ccsv5

$ sudo ./uninstall_CCSv5

2. After 30 minutes, the un-installation process seemed to hang so I had to kill it,

3. I've manually removed the remaining folders:

$ cd /opt

$  rm -rfv ti/*

4. I've successfully re-installed CCSV5.

5. Where is the file "install_drivers.sh" as mentioned in the readme.txt file?

  I've found another file "ti_xds100_linux_install.sh" in the folder "/opt/ti/ccsv5/ccs_base/common/uscif/install/" - Not sure it's correct.

Regards,

g

-------------------

Solved:

Re-install "CCSV5.3 + all feature option" using the online-installer option is correctly installing: /opt/ti/ccsv5/install_scripts/install_drivers.sh.

The shell script folder never got created with the Linux-offline installer twice + custom setup - weird (installation bug?)