I have imported ccs v3.3 project into ccs v5.3, I am getting following errors. I have the library path specified in project setting.
"C:/ti/MyProjects/F2808/FC00_03_21/cmd\Flash2808_API_V302.lib<Flash28_Erase.
obj>": compatibility cannot be determined
warning #16002-D: build attribute vendor section TI missing in
"C:/ti/MyProjects/F2808/FC00_03_21/cmd\Flash2808_API_V302.lib<Flash28_EraseS
ector.obj>": compatibility cannot be determined
warning #16002-D: build attribute vendor section TI missing in
"C:/ti/MyProjects/F2808/FC00_03_21/cmd\Flash2808_API_V302.lib<Flash28_Global
s.obj>": compatibility cannot be determined
warning #16002-D: build attribute vendor section TI missing in
:
:
Please help! Have have also attached the cmd file and library file its complaining about.
Thanks
Prasoon
/*
//###########################################################################
//
// FILE: F2808.cmd
//
// TITLE: Linker Command File For F2808 Device
//
//###########################################################################
// $TI Release: DSP280x, DSP2801x Header Files V1.41 $
// $Release Date: August 7th, 2006 $
//###########################################################################
*/
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP280x_Headers\cmd
//
// For BIOS applications add: DSP280x_Headers_BIOS.cmd
// For nonBIOS applications add: DSP280x_Headers_nonBIOS.cmd
========================================================= */
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */
/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP280x_Headers_nonBIOS.cmd */
/* Uncomment this line to include file only for BIOS applications */
/* -l DSP280x_Headers_BIOS.cmd */
/* 2) In your project add the path to <base>\DSP280x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */
/* Define the memory block start/length for the F2808
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F2808 are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
L0/L1 and H0 memory blocks are mirrored - that is
they can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.
Contiguous SARAM memory blocks or flash sectors can be
be combined if required to create a larger memory block.
*/
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
/*RAML0 : origin = 0x008000, length = 0x000400 /* on-chip RAM block L0 */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PRAML1 : origin = 0x3F9C00, length = 0x001700 /* on-chip RAM block L1 */
PRAMH0 : origin = 0x3FB300, length = 0x000C00 /* on-chip RAM block H0 */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
BOOT_RSVD : origin = 0x000400, length = 0x000080 /* Part of M1, BOOT rom will use this for stack */
RAMM1 : origin = 0x000480, length = 0x000380 /* on-chip RAM block M1 */
/*RAML0 : origin = 0x008400, length = 0x000C00 /* on-chip RAM block L0 */
RAML0 : origin = 0x008000, length = 0x001C00 /* on-chip RAM block L0 */
/*RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
DRAMH0 : origin = 0x3FBF00, length = 0x000100 /* on-chip RAM block H0 */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = PRAML1,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
{
-l cmd\Flash2808_API_V302.lib(.econst)
-l cmd\Flash2808_API_V302.lib(.text)
}
ramfuncs2 : LOAD = FLASHD,
RUN = PRAMH0,
LOAD_START(_Ramfuncs2LoadStart),
LOAD_END(_Ramfuncs2LoadEnd),
RUN_START(_Ramfuncs2RunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > RAML0 PAGE = 1
.ebss2 : > DRAMH0 PAGE = 1
.esysmem : > DRAMH0 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHC PAGE = 0
.switch : > FLASHC PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHC PAGE = 0 /* Math Code */
IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/