Other Parts Discussed in Thread: CCSTUDIO
Hi,
I installed code composer studio 5.3.0 in ubuntu 12.04, after installation i was able to get a desktop icon with a lock symbol along with it, when i double clicked it css started but it crashed then i started it in command prompt with sudo command, but again it crashed after a few minutes.
from the terminal I obtained the following information during the crash as,
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
flxInitLoad: client has not been protected.
No bp log location saved, using default.
[000:000] Browser XEmbed support present: 1
[000:001] Browser toolkit is Gtk2.
[000:001] Using Gtk2 toolkit
[000:308] Warning(optionsfile.cc:47): Load: Could not open file, err=2
[000:308] No bp log location saved, using default.
[000:308] Browser XEmbed support present: 1
[000:308] Browser toolkit is Gtk2.
[000:308] Using Gtk2 toolkit
java version "1.6.0_24"
OpenJDK Runtime Environment (IcedTea6 1.11.5) (6b24-1.11.5-0ubuntu1~12.04.1)
OpenJDK Server VM (build 20.0-b12, mixed mode)
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
what could be the problem here, could you please help.
thanks,
Haneef