Hi all:
We have a University Floating Site License CCS 5 (TMDSCCS-ALLUNVF100-v5),
and we do not know how to configure the CCS client to connect to the license
server.
We have installed the license server according to the document "License Server
Administration for CCS". According to the LMTOOLS utility, the server is up and
running, with the following System Information:
Computer/Hostname: LEP15
IP address: 192.168.0.38
Ethernet address: 00e07df8f0cb
Port: 27000
Within the CCS clients, when selecting:
Help -> Code Composer Studio Licensing Information -> Upgrade -> Launch
License Setup -> ACTIVATE -> Next> -> Specify a license server
We get a dialog window asking for the Address and Port. We have tried many combinations
(LEP15, 192.168.0.38 etc. etc., and 27000 for the port) but we did not succeed, and the CCS
client is in the 90 days trial mode.
We have verified Windows firewall configurations in both the server and the cilent, and all
seems to be OK. All computers are running Windowx XP Pro.
Any help with the Address and Port configurations are welcomed.
Thanks,
Wilson