I try connect host PC (windows ip:192168.0.1) with linux(ip:192.168.0.3) on TCI6638 Keystone2 Device Simulator.
On wireshark I seen ARP packet with wrong sequence number:
This is some bug in simulator ? or I doing something wrong ?
Packet from linux are delivered to windows but linux don’t gets packets from windows.
Could somebody write me how to connect simulator with windows? How to test connection (ping function work or not ?)?
Thanks in advance,
Jakub