This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4: configuration of flash sectors is lost

Hello,

I am using CCS4 for F28069U development. I have noticed that whenever I import an exiting project to a new workspace, the flash sector configuration is lost.

more details: suppose I configure sectors A, B to be erased on connection to target. it works as long as I work in the same workspace. If I import this project to another workspace, this configuration is lost and as soon as I connect to target, all sectors are erased.

could some one help in correcting this?

thank you,

Vishwanatha

  • Hi Vishwanatha,

    unfortunately, as you have discovered, there are settings that are not saved across workspaces.   The best you can do is the following

    - use the same ccxml (target configuration file)

    - see what settings you may be able to preserve unde File->Export->General->Project PReferences.


    This may still not preserve everything.

    Sorry for the inconvenience and hope this clarification will help.

    Best Regards,
    Lisa