This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

setting compiler option for DSK6713 in ccs v5.2?

i m using ccs v5.2 for DSK6713 i have got compilation error ....

tell me initialization for compiler....

 i have taken refrence from link:-  http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/215890.aspx

**** Build of configuration Debug for project sine8_led ****

 

C:\ti\ccsv5\utils\bin\gmake -k all

'Building file: ../main.c'

'Invoking: C6000 Compiler'

"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/bin/cl6x" -mv-mv6700 -g --define=-D"CHIP_6713" --define=define=CHIP_6713 --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/bios/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/dsk6713/lib" --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/dsk6713/include" --display_error_number --diag_warning=225 --abi=coffabi --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"

>> WARNING: invalid version 0, defaulting to 6200

Command-line error #1046: invalid macro definition: -DCHIP_6713

1 fatal error detected in the compilation of "../main.c".

Compilation terminated.

 

>> Compilation failure

gmake: *** [main.obj] Error 1

'Building file: ../vector_poll.asm'

'Invoking: C6000 Compiler'

"C:/ti/ccsv5/tools/compiler/c6000_7.3.4/bin/cl6x" -mv-mv6700 -g --define=-D"CHIP_6713" --define=define=CHIP_6713 --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/bios/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/dsk6713/lib" --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.3.4/include" --include_path="C:/ti/ccsv5/DSK6713/DSK6713/c6000/dsk6713/include" --display_error_number --diag_warning=225 --abi=coffabi --preproc_with_compile --preproc_dependency="vector_poll.pp"  "../vector_poll.asm"

>> WARNING: invalid version 0, defaulting to 6200

'Finished building: ../vector_poll.asm'

' '

gmake: Target `all' not remade because of errors.

 

**** Build Finished ****