This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer 5.1.1.00033 for Linux uses Windows debug command



Hi,

     We are trying to debug u-boot in the following environment:

     - Ubuntu 12.0 64 bit (needed to add the 32 bit libraries, sudo apt-get install ia32-lib)

     - TI SDK 05.06.00.00

     - Code Composer 5.1.1.00033 for Linux

     - Blackhawk XDS560v2-USB System Trace Emulator

   u-boot is imported and target configuration file is created. When I try to "Test Connection" I get the following error:

     Why is Code Composer looking for the Windows version of the jtag debug executable (dbgjtag.exe)? Is there a quick fix for this?

Thanks,

     John C.