Hi,
Is there a way of moving CCS5.5.3.0 project from one computer to another?
Following the wiki http://processors.wiki.ti.com/index.php/Project_Sharing I did the following simple exercise:
1) imported the qs-logger project from C:\StellarisWare\boards\ek-lm4f232\qs-logger with an option of "copy projects into workspace" enabled
and "Automatically import referenced projects" enabled as well. It builds OK with only a couple of warnings, but creates a numer of link files instead of copying real files.
2) exported the project as general Archive File, selected all and saved in zip format
3) switched to a new workspace and imported selecting an archive file from the previous step
4) rebuilding the imported project fails as it has a number of missing files.
Questions:
1) Is there another way to achieve what I want?
2) What is the easiest procedure to fix that problem?
Regards
Jan