Other Parts Discussed in Thread: TMS320C6726B
Back in March of 2009, I purchased a 'Platimun' license for CCS. I think I received a license file for v4.x of CCS in 2010. I still have the CCS IDE 'Service Code' number, if that helps.
All I have used so far is CCS v3.3 on a Windows XP platform, to build code for a TMS320C6726B DSP chip.
I would like to start development work using a Stellaris Cortex-M3 or M4 chip. Does CCS v5.3 include a compiler for the Cortex-Mx series chips? If so, then how do I upgrade my license to support CCS v5.3 (if that is your latest version)?
I plan to run CCS v5.3 on a Windows 7, 64-bit machine, with 8GB of RAM.
Is there a debugger pod I need for making the JTAG connection to the target machine? I have an XDS510 USB Plus, from Spectrum Digital - will that work?
Thanks,
Steve