Other Parts Discussed in Thread: MSP430WARE
Hi,
I've recently acquired a launchpad MSP430 and launchpad Stellaris. I note that CCS comes as a simple 5.3 version (and from my understanding this includes the MSP430ware with GUI). The MSP430ware is available separately but without GUI.
For the Stellaris there is a standalone Stellarisware package or the CCS with Stellarisware.
The computer I plan to install the software on is a little ancient and when I install the CCS5.3 it felt as thought it took forever (at least an 1 hour). So to avoid another long install, can I just install the standalone stellarisware on the PC having the CCS5.3 and have both the Stellarisware and MSP430ware available on the same CCS package?
After installing CCS5.3 I noted that there are 4 licence options, the last being "code limited (MSP430)" and the penultimate is "free license". Will I see a "code limited (stellaris)" when I install the stellarisware? It would appear that I may be able to swap between these license options on the help menu? One last question: what is the difference between "free license" and "code limited"?
Thanks for the help.
Neil