This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it possible to wakeup dsp from reset without Gelfile in DM8148?

Hi All,

we are using DM814X board for our project. When we connect target to the emulator, we right clicked on CORTEXA8 and made connect target. Then when we tried connecting DSP, it produces error like

C674X_0:Error connecting to the target :Error 0X80000240/-1180 Fatal Error during:Initializion ,OCS,The target is being held in reset.The applied reset must be released before progressing.


Note: These process is done with no gel files.

Regards,

K.AmirthaRaj