This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem regarding .asm file

Hi,

I am using C5515. It has an Hardware FFT Accelarator.

I got the hwafft_rom.asm, hwafft.asm and hwafft.h

I used a sample code given in TI documentation for FFT implementation.

But, I am not able to link .asm files to the project.

I feel .asm files will be converted to .obj after building. But, I cant see any of my .asm files being converted to .obj

Maybe because of this I am getting a [E0000]: Parse error when i buidl

Can u plz help me out

  • Hi,

    Can you copy the full console output to a text file and attach to your post? This goes a long way to help diagnosing this issue.

    Regards,

    Rafael

  • Thankx for the reply.

    I had those issues. But I just played arround with the files and somehow came out of it. Now, I dont have any errors ( except four warnings).
    But, when i am running the code, I am not able to get the FFT computed. As soon as the code reaches the FFT computation part, it just stands still.
    So , I stopped the running to see what is getting executed. The code gets stuck here

    8e49bdeb1110             COPR #16,AC0,dbl(*AR2-),AC1 :: MOV AC1,dbl(*(AR3+T0))
    8e49bdeb1110             COPR #16,AC0,dbl(*AR2-),AC1 :: MOV AC1,dbl(*(AR3+T0))
    8e49bdeb1110             COPR #16,AC0,dbl(*AR2-),AC1 :: MOV AC1,dbl(*(AR3+T0))
    8e49bdeb1110             COPR #16,AC0,dbl(*AR2-),AC1 :: MOV AC1,dbl(*(AR3+T0))

    I am not sure , what exactly these statements does. But all the lines are same !!

    If i step debug this, it loops arround these lines.

    But, If i give a run and stop , it get stuck @

    040009                   BCC #0x3d12c3,AC0 == #0

    and if I give a run again : I get an error message saying I cant do tht !!!!!!

    I am struggling with this issue for the past 2-3 days. It will be a great help, If you can tell me how to solve this.
    I have a breif code structure, which shows how I am computing FFT. Please have a look.

    This is my code
    ==================================================================================================================================
    #include "stdio.h"
    #include "usbstk5515.h"
    #include "usbstk5515_led.h"
    #include "usbstk5515_gpio.h"
    #include "usbstk5515_i2c.h"
    #include "sar.h"
    #include "lcd.h"
    #include "hwafft.h"
    #include "math.h"

    Int32 Input_Signal1024];
    extern Uint16 hwafft_wrapper(  Int32 *data,Int32 *scratch,Uint16 fft_flag,Uint16 scale_flag,hwafft_func_t fft_func);
    Int32* fft(Int32 *data);

    void main( void )
    {
        Int16 result = 0;Int32 *fft_data = 0;
        USBSTK5515_init( );
        Input_Signal =  Aquire_signal_from_ADC_for_10s();
        fft_data = fft( Input_Signal);
        while(1);
    }

    Int32* fft(Int32 *data)
    {
        Int32 *result = 0;
        Int32 *data_br = 0;
        Uint16 out_sel = 0;
        Int32 *scratch=  0;
        hwafft_br(data,data_br,DATA_LEN_1024); // bit reversal
        data = data_br;
        out_sel = hwafft_wrapper(data,scratch,FFT_FLAG,SCALE_FLAG,hwafft_1024pts); // I am using this because, I am using large memory model
        if (out_sel == OUT_SEL_DATA)
        {
            result = data;
        }
        else
        {
            result = scratch;
        }        
        return(result);
    }   
    ===================================================================================================================================
    ===================================================================================================================================

    I have defined the below code in an assembly file. I got this code snippet from TI forum. I was asked to use this since I am using large memory model. It seems
    FFT accelerator supports only small memory model

             .sect ".onchip_code"
             .def _hwafft_wrapper
            ; HWAFFT code burned in C5515 ROM seems to support small memory model only.
            ; The following wrapper helps to use HWAFFT for large/huge memory models.
            ; CVN 20110920
    _hwafft_wrapper:
        XAR2 = XAR1
        XAR3 = XAR0
        call AC0
        return

    I have defined the below code in a C header file.(USBSTK5515.h)

    typedef Uint16 (*hwafft_func_t)(Int32 *data,
                                    Int32 *scratch,
                                    Uint16 fft_flag,
                                    Uint16 scale_flag);
    Uint16 hwafft_wrapper(  Int32 *data,
                            Int32 *scratch,
                            Uint16 fft_flag,
                            Uint16 scale_flag,
                            hwafft_func_t fft_func);


    ===================================================================================================================================
    ===================================================================================================================================

    The following is my .cmd file

    -stack    0x400                /* PRIMARY STACK SIZE    */
    -sysstack 0x400                /* SECONDARY STACK SIZE  */
    -heap     0x400               /* HEAP AREA SIZE        */  
    MEMORY
    {
        MMR     (RW) : origin = 0000000h length = 0000c0h     /* MMRs */
        DARAM_0 (RW)  : origin = 00000c0h length = 001f40h    /* on-chip DARAM 0 */
        DARAM_1 (RW)  : origin = 0002000h length = 002000h    /* on-chip DARAM 1 */
        DARAM_2 (RW)  : origin = 0004000h length = 002000h    /* on-chip DARAM 2 */
        DARAM_3 (RW)  : origin = 0006000h length = 002000h    /* on-chip DARAM 3 */
        DARAM_4 (RW)  : origin = 0008000h length = 002000h    /* on-chip DARAM 4 */
        DARAM_5 (RW)  : origin = 000a000h length = 002000h    /* on-chip DARAM 5 */
        DARAM_6 (RW)  : origin = 000c000h length = 002000h    /* on-chip DARAM 6 */
        DARAM_7 (RW)  : origin = 000e000h length = 002000h    /* on-chip DARAM 7 */
        SARAM   (RW) : origin = 0010000h length = 040000h    /* on-chip SARAM */
        SAROM_0 (RX)  : origin = 0fe0000h length = 008000h     /* on-chip ROM 0 */
        SAROM_1 (RX)  : origin = 0fe8000h length = 008000h     /* on-chip ROM 1 */
        SAROM_2 (RX)  : origin = 0ff0000h length = 008000h     /* on-chip ROM 2 */
        SAROM_3 (RX)  : origin = 0ff8000h length = 007f00h     /* on-chip ROM 3 */
        VECS    (RX)  : origin = 0ffff00h length = 000100h    /* on-chip ROM vectors */
        EMIF_CS0 (RW) : origin = 0050000h  length = 07B0000h    /* mSDR */
        EMIF_CS2 (RW) : origin = 0800000h  length = 0400000h    /* ASYNC1 : NAND */
        EMIF_CS3 (RW) : origin = 0C00000h  length = 0200000h    /* ASYNC2 : NAND  */
        EMIF_CS4 (RW) : origin = 0E00000h  length = 0100000h    /* ASYNC3 : NOR */
        EMIF_CS5 (RW) : origin = 0F00000h  length = 00E0000h    /* ASYNC4 : SRAM */
    }
    SECTIONS
    {
        vectors (NOLOAD)
        .intvec                         : > DARAM_0        ALIGN = 256
        .bss                             : > SARAM         /*, fill = 0 */
        .stack                           : > DARAM_1     ALIGN = 1024
        .sysstack                    : > DARAM_1     ALIGN = 1024
        .heap                          : > DARAM_1        ALIGN = 1024
        .text                              : > SARAM          ALIGN = 1024
        .onchip_code            : > SARAM
         .cinit                            : > DARAM_2
        .cio                                : > DARAM_2
        .const                            : > DARAM_2
        
    // The Bit-Reverse destination buffer data_br_buf requires an address with
    // at least 4+log2(FFT_LENGTH) least significant binary zeros

        data_br_buf          : > DARAM_1        ALIGN = 1024
        scratch_buf           : > DARAM_1        ALIGN = 1024
        convolved_buf       : > DARAM_2
        coeffs_fft_buf         : >    DARAM_2

        RcvL1            : > DARAM_3    
        RcvL2            : > DARAM_3    
        RcvR1            : > DARAM_4    
        RcvR2            : > DARAM_4    

        FilterOut    : > DARAM_5    
        OverlapL    : > DARAM_5    
        OverlapR    : > DARAM_5    

        XmitL1        : > DARAM_6    
        XmitL2        : > DARAM_6    
        XmitR1        : > DARAM_7    
        XmitR2        : > DARAM_7    

        RcvL1_copy    : > SARAM    
        RcvL2_copy    : > SARAM    
        RcvR1_copy    : > SARAM    
        RcvR2_copy    : > SARAM    

        .emif_cs0   : > EMIF_CS0
        .emif_cs2   : > EMIF_CS2
        .emif_cs3   : > EMIF_CS3
        .emif_cs4   : > EMIF_CS4
        .emif_cs5   : > EMIF_CS5
    }

    ===================================================================================================================================
    ===================================================================================================================================

    Following is my console output:


    **** Build of configuration Debug for project first_Project ****

    E:\TI\ccsv4\utils\gmake\gmake -k all
    'Building file: ../csl_irqplug.asm'
    'Invoking: Compiler'
    "E:/TI/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --include_path="E:/TI/xdais_6_25_01_08/packages/ti/xdais" --include_path="E:/C5505/CD/C5505/Chapter 1/Application 1 Getting Started" --include_path="E:/TI/ccsv4/emulation/boards/usbstk5515_v1/include" --include_path="E:/TI/ccsv4/tools/compiler/c5500/include" --include_path="E:/TI/bios_5_41_02_14" --include_path="E:/TI/bios_6_21_00_13" --include_path="E:/C5505/CSL/build" --include_path="E:/C5505/CSL/inc" --include_path="E:/C5505/CSL/src" --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic --preproc_with_compile --preproc_dependency="csl_irqplug.pp"  "../csl_irqplug.asm"
    'Finished building: ../csl_irqplug.asm'
    ' '
    'Building file: ../main.c'
    'Invoking: Compiler'
    "E:/TI/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --include_path="E:/TI/xdais_6_25_01_08/packages/ti/xdais" --include_path="E:/C5505/CD/C5505/Chapter 1/Application 1 Getting Started" --include_path="E:/TI/ccsv4/emulation/boards/usbstk5515_v1/include" --include_path="E:/TI/ccsv4/tools/compiler/c5500/include" --include_path="E:/TI/bios_5_41_02_14" --include_path="E:/TI/bios_6_21_00_13" --include_path="E:/C5505/CSL/build" --include_path="E:/C5505/CSL/inc" --include_path="E:/C5505/CSL/src" --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"
    "E:\TI\ccsv4\emulation\boards\usbstk5515_v1\include\usbstk5515.h", line 144: warning: typedef name has already been declared (with same type)
    "E:\TI\ccsv4\emulation\boards\usbstk5515_v1\include\usbstk5515.h", line 144: warning: typedef name has already been declared (with same type)
    "E:\TI\ccsv4\emulation\boards\usbstk5515_v1\include\usbstk5515.h", line 144: warning: typedef name has already been declared (with same type)
    "E:/TI/ccsv4/emulation/boards/usbstk5515_v1/include/usbstk5515.h", line 144: warning: typedef name has already been declared (with same type)
    "../main.c", line 33: warning: integer conversion resulted in a change of sign
    "../main.c", line 34: warning: integer conversion resulted in a change of sign
    "../main.c", line 341: warning: last line of file ends without a newline
    'Finished building: ../main.c'
    ' '
    'Building file: ../sample_code.c'
    'Invoking: Compiler'
    "E:/TI/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --include_path="E:/TI/xdais_6_25_01_08/packages/ti/xdais" --include_path="E:/C5505/CD/C5505/Chapter 1/Application 1 Getting Started" --include_path="E:/TI/ccsv4/emulation/boards/usbstk5515_v1/include" --include_path="E:/TI/ccsv4/tools/compiler/c5500/include" --include_path="E:/TI/bios_5_41_02_14" --include_path="E:/TI/bios_6_21_00_13" --include_path="E:/C5505/CSL/build" --include_path="E:/C5505/CSL/inc" --include_path="E:/C5505/CSL/src" --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic --preproc_with_compile --preproc_dependency="sample_code.pp"  "../sample_code.c"
    At end of source: warning: a translation unit must contain at least one declaration
    'Finished building: ../sample_code.c'
    ' '
    'Building file: ../vectors.asm'
    'Invoking: Compiler'
    "E:/TI/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --include_path="E:/TI/xdais_6_25_01_08/packages/ti/xdais" --include_path="E:/C5505/CD/C5505/Chapter 1/Application 1 Getting Started" --include_path="E:/TI/ccsv4/emulation/boards/usbstk5515_v1/include" --include_path="E:/TI/ccsv4/tools/compiler/c5500/include" --include_path="E:/TI/bios_5_41_02_14" --include_path="E:/TI/bios_6_21_00_13" --include_path="E:/C5505/CSL/build" --include_path="E:/C5505/CSL/inc" --include_path="E:/C5505/CSL/src" --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic --preproc_with_compile --preproc_dependency="vectors.pp"  "../vectors.asm"
    'Finished building: ../vectors.asm'
    ' '
    'Building target: first_Project.out'
    'Invoking: Linker'
    "E:/TI/ccsv4/tools/compiler/c5500/bin/cl55" -vcpu:3.3 -g --diag_warning=225 --ptrdiff_size=32 --algebraic --memory_model=large --asm_source=algebraic -z -m"first_Project.map" --warn_sections -i"E:/TI/ccsv4/tools/compiler/c5500/lib" -i"E:/C5505/CSL/first_Project/../../lib" -i"E:/TI/ccsv4/tools/compiler/c5500/include" --reread_libs --rom_model -o "first_Project.out"  "./vectors.obj" "./sample_code.obj" "./main.obj" "./csl_irqplug.obj" -l"E:\TI\ccsv4\tools\compiler\c5500\lib\rts55x.lib" -l"E:\C5505\CD\C5505\Chapter 1\Application 1 Getting Started\55xdsph.lib" -l"E:\C5505\CSL\build\cslVC5505.lib" -l"E:\TI\ccsv4\tools\compiler\c5500\lib\lib\usbstk5515bsl.lib" "../C5515.cmd"
    <Linking>
    'Finished building target: first_Project.out'
    ' '
    Build complete for project first_Project