This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Probelem while using Crash Dump Analysis

Hi, all,

I'm working with C674x and CCS5.3. Now I met a problem while using Crash Dump Analysis.

I followed the instructions in http://processors.wiki.ti.com/index.php/Crash_Dump_Analysis to do the crash dump analysis.
When I typed the following command in the Scripting Console, it reported such error:

Initializing ... (Completed)

js:> eval "GEL_SystemRestoreState(\"D:\\test_dss.txt\")"
org.mozilla.javascript.EvaluatorException: illegal character
js:>

The data file is something like the following:

521177 103
R A0 0x0000000B 0x00000001
......
M 0x00000000 0x8B0161B0 0x184
0x02
0xCD
......

Is there anything I miss ?

Thanks.