hello,
I am currently using code composer studio v 3.1 to connect to C6713 DSK. Since I have Win 7 I run the Code Composer Studio in Win XP mode. It works fine most of the time, but some times its crashes giving the following error,
"Trouble running Target CPU: Error 0x800020A0/-1220 Fatal Error during: Execution, Target Communication, Control, Device driver: Lost USB connection to emulator. You should ABORT and restart to re-establish the USB link. Sequence ID: 16 Error Code: -1220 Error Class: 0x800020A0
Failed to remove the debug state from the target before disconnecting. There may still be breakpoint opcodes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging."
This appears to happen when the PC is doing memory intensive thing like running Matlab code that uses a lot of memory. Every time this happens I have to shut down the the code composer, the Win XP mode window and unplug and repower the DSK. Can any please suggest if there is a way to avoid this error.
Best regards,
Umar Khan.