This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue building with MSP430 C/C++ v4.1.5

Other Parts Discussed in Thread: MSP430FR5949

I have a CCSv5 project that builds with no problems using MSP430 compiler version 4.1.3.  When I build with compiler version 4.1.5, I get several errors during linking like this. 

"../lnk_msp430fr5949.cmd", line 105: error #10100-D: conflicting placement
   methods specified for "PARAMS_SEG"
"../lnk_msp430fr5949.cmd", line 105: error #10026-D: expecting output section,
   GROUP, or UNION instead of ":"
The offending lines in my lnk.cmd file are:

From MEMORY:

MEMORY
{
    SFR                     : origin = 0x0000, length = 0x0010
    PERIPHERALS_8BIT        : origin = 0x0010, length = 0x00F0
    PERIPHERALS_16BIT       : origin = 0x0100, length = 0x0100
    RAM                     : origin = 0x1C00, length = 0x0800
    PARAMS_SEG              : origin = 0x1800, length = 0x0080  /* INFOA used for params */
    EXCEPTION_LOG_SEG       : origin = 0x1880, length = 0x0080
    INFOC                   : origin = 0x1900, length = 0x0050 /* Shortened to allow other sections to use some info memory */
    PGM_Q_SEG               : origin = 0x1950, length = 0x0010
    SEC_LOG_SEG             : origin = 0x1960, length = 0x00A0
 ......

From SECTIONS:

SECTIONS
{
      PARAMS_SEG         : > PARAMS_SEG
      PGM_Q_SEG         : > PGM_Q_SEG

the error is for line 105, the line with PGM_Q_SEG.....

Is there a change in 4.1.5 that I need to understand better?  The release notes talked about this:

------------------------------------------------------------------------------
FIXED  SDSCM00032000
------------------------------------------------------------------------------

Summary            : linker should not allows type flags on GROUP/UNION

Fixed in           : 4.1.5
Severity           : S3 - Minor
Affected Component : Linker

Description:
Update linker command file parser to disallow the type keyword if applied to a
GROUP or UNION.

but I don't know if this is my problem