Other Parts Discussed in Thread: OMAP-L138, SYSBIOS, CCSTUDIO
Team,
I am using CCS 5.3.0.00090 under Win XP SP3.
So far I was able to use SW breakpoints without problems to debug the audio example from the SYSBIOS PSP 3.01 on C674x CPU of the OMAP-L138.
I could place SW breakpoint in:
- .c file part of the project (like audioSample_io.c)
- .c file from the McASP SYSBIOS driver that are not part of the project but that are the src file of the .lib is used in the project (like mcasp.c, mcasp_edma.c).
Now I can still place breakpoints in audioSample_io.c. However when I use breakpoint in the mcasp.c, mcasp_edma.c I get the following Message log. The breakpoint seem to be placed but CPU does not seem to always stop. I am not sure if the breakpoint behavior is consistent.
Any idea of what the message log means?
Thanks and best regards,
Anthony
eclipse.buildId=I20120608-1200
java.version=1.6.0_13
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Framework arguments: -product com.ti.ccstudio.branding.product
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.ti.ccstudio.branding.product
Error
Wed Mar 13 15:56:58 GMT 2013
msg.error.UnknownException
java.lang.NullPointerException
at org.eclipse.rtsc.xdctools.model.ui.editors.CCSChangeListener.resourceChanged(Unknown Source)
at org.eclipse.core.internal.events.NotificationManager$1.run(NotificationManager.java:291)
at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
at org.eclipse.core.internal.events.NotificationManager.notify(NotificationManager.java:285)
at org.eclipse.core.internal.events.NotificationManager.broadcastChanges(NotificationManager.java:149)
at org.eclipse.core.internal.resources.Workspace.broadcastPostChange(Workspace.java:395)
at org.eclipse.core.internal.resources.Workspace.endOperation(Workspace.java:1530)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2353)
at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2326)
at com.ti.ccstudio.debug.internal.breakpoint.CCSBreakpoint.run(CCSBreakpoint.java:254)
at com.ti.ccstudio.debug.internal.breakpoint.CCSBreakpoint.<init>(CCSBreakpoint.java:240)
at com.ti.ccstudio.debug.internal.breakpoint.CCSBreakpoint.<init>(CCSBreakpoint.java:105)
at com.ti.ccstudio.debug.internal.ui.breakpoint.togglers.EditorToggleBreakpointsTarget.insertBreakpoint(EditorToggleBreakpointsTarget.java:155)
at com.ti.ccstudio.debug.internal.ui.breakpoint.togglers.EditorToggleBreakpointsTarget.toggleLineBreakpoints(EditorToggleBreakpointsTarget.java:71)
at com.ti.ccstudio.debug.internal.ui.breakpoint.togglers.EditorToggleBreakpointsTarget.toggleBreakpoints(EditorToggleBreakpointsTarget.java:59)
at org.eclipse.debug.ui.actions.ToggleBreakpointAction.doIt(ToggleBreakpointAction.java:119)
at org.eclipse.debug.ui.actions.ToggleBreakpointAction.runWithEvent(ToggleBreakpointAction.java:89)
at org.eclipse.debug.ui.actions.RulerToggleBreakpointActionDelegate.runWithEvent(RulerToggleBreakpointActionDelegate.java:123)
at org.eclipse.ui.internal.handlers.ActionDelegateHandlerProxy.execute(ActionDelegateHandlerProxy.java:281)
at org.eclipse.core.commands.Command.executeWithChecks(Command.java:499)
at org.eclipse.core.commands.ParameterizedCommand.executeWithChecks(ParameterizedCommand.java:508)
at org.eclipse.ui.actions.ContributedAction.runWithEvent(ContributedAction.java:185)
at org.eclipse.ui.texteditor.AbstractTextEditor$14.triggerAction(AbstractTextEditor.java:3074)
at org.eclipse.ui.texteditor.AbstractTextEditor$14.mouseDoubleClick(AbstractTextEditor.java:3100)
at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:196)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4169)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3758)
at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2701)
at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2665)
at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2499)
at org.eclipse.ui.internal.Workbench$7.run(Workbench.java:679)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:124)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:110)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:79)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:353)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:180)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:629)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:584)
at org.eclipse.equinox.launcher.Main.run(Main.java:1438)