This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.4.0 Beta 1 - can not install NDK package of MCSDK

Hi,

I just installed CCS 5.4.0 Beta 1 which worked fine basically.

After installing MCSK bios_mcsdk_02_01_02_05_setupwin32 it happens that the ndk package installation is refused.

All other MCSDK packages were installed properly.

I tried with different versions of ndk, ndk_2_21_01_38 and ndk_2_21_03_2, with same result.

An error occurred while collecting items to be installed
session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=)
Problems downloading artifact: osgi.bundle,com.ti.rtsc.NDK.product_2.21.1.38,2.21.1.38.
File has invalid content:C:\Users\hahna\AppData\Local\Temp\signatureFile6777766244511778256.jar
      Invalid content:plugin.xml
      The file "plugin.xml" in the jar "C:\Users\hahna\AppData\Local\Temp\signatureFile6777766244511778256.jar" has been tampered!

Screenshots attached.

best regards

Alois