Hi all I am having an issue with Code Composer. I am running version 3.3.82.13 and I am programming to an F28335. I have an old version of software and when I directly program it to the DSP the ADC works. However. if I load the project code into CCS, don't change a thing, recompile build, and then program the DSP, the ADC does not work. Is there something wrong with my compiler or setting that is causing this error?