Hi everybody
i have a problem with CSS 5.3, first i want to program a stellaris launchpad board, the problem is :
Afther the installation of eclipse, stellariswave etc,
I try to run an exemple "project0" when i do it i have that error in eclipse :
Error initializing emulator:
Error loading libdebug.so. Please make sure that the file exists (/home/cyber37/ti/ccsv5/ccs_base/DebugServer/drivers/libdebug.so)
Thanks for help,
The libdebug file is in the path and working (i tested with ldd)
I schearch on google i see no solution, so can we fix the problem now ?? And how pleaze ?