Other Parts Discussed in Thread: MSP430F67791
Does anyone know wher I can obtain the C header file and linker script for the msp430f67791? I have tried updating software but that did not help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F67791
Does anyone know wher I can obtain the C header file and linker script for the msp430f67791? I have tried updating software but that did not help.
Hi Steve,
do you not see the file in this path of your installation?
C:\CCS\5_3\ccsv5\ccs_base\msp430\include
This is from a normal v5.3 installation and the file is there on my install. If the file is not there in your case. Could you please confirm you have CCS with msp430 support installed and could you also double check for permissions/antivirus issues.
Best Regards,
Lisa
Thanks for your reply, Lisa. I do not see the files in my installation (C:\ti\ccsv5\ccs_base\msp430\include). I msp430 support ( we use several other msp 430s). I am running version 5.1.0.09000. I updated, but all installs failed after the download with no indication as to why. I tried to update again, but now receive an indication that no updates are available.
Hi Steve,
I would do a full fresh installation of v5.3 into a clean simple directory. There are unfortunately many known issues with updating from these old versions.
You should then have many bug fixes, updates and support for this device automatically.
Please keep us informed how it goes.
Best Regards,
LIsa