Other Parts Discussed in Thread: TMS320C6747
Dear Sir,
I used TMS320C6747 processor and i tried to get sine waveform(via DAC without ADC) using matlab simulink model and m-file.Project was created in CCS studio but while load a program below mention errors are displayed.Please solve this errors
In CCS STUDIO:
MATLAB:
1.The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while loading and running the project.
The build process will terminate as a result
2.Error while loading and running the project.
3.There was a problem loading the COFF file.
Make sure that the build was successful and that the selected board is of the correct type.
Advance thanks,
Vignesh